Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-29 05:57 AM
This was originally posted on APC forums on 1/11/2017
Hi
I foolishly purchased the above device thinking it had a slot for an SNMP card, but when I got it I realised it doesn't.
So I'm trying to run apcupsd to monitor the device. Powerchute looks like it has all the useful info like Line in, Line out, etc. but the apcupsd output seems very limited. i.e. See below. I get no indication of linve voltage in or out, load power or anything else.
Please can you advise? It seems very much more limited than even the £80 APC devices I've been using in the past.
root@ibworth-pi:/etc/apcupsd# apcaccess
APC : 001,027,0668
DATE : 2017-01-11 15:58:21 +0000
HOSTNAME : ibworth-pi
VERSION : 3.14.14 (31 May 2016) debian
UPSNAME : ibworth-pi
CABLE : USB Cable
DRIVER : USB UPS Driver
UPSMODE : Stand Alone
STARTTIME: 2017-01-11 15:58:19 +0000
MODEL : Smart-UPS C 1500
STATUS : ONLINE
BCHARGE : 100.0 Percent
TIMELEFT : 297.0 Minutes
MBATTCHG : 5 Percent
MINTIMEL : 3 Minutes
MAXTIME : 0 Seconds
ALARMDEL : 30 Seconds
BATTV : 27.3 Volts
NUMXFERS : 0
TONBATT : 0 Seconds
CUMONBATT: 0 Seconds
XOFFBATT : N/A
STATFLAG : 0x05000008
MANDATE : 2016-08-17
SERIALNO : 3S1632X07908
NOMBATTV : 24.0 Volts
FIRMWARE : UPS 10.0 / ID=1005
END APC : 2017-01-11 15:58:24 +0000
Posted: 2021-06-29 05:57 AM
This reply was originally posted by Jervee on APC forums on 1/12/2017
In my experience, I think that its all there is the unit can offer. Actually, you can see in the LCD Display of the unit the input and output voltage, you'll just have to manually check it in front of your unit. With regards to the NMC Slot of your unit, unfortunately, that's all there is. I wish that you'd purchased the SMT Model because even the 750VA ones has an NMC Card slot.
Posted: 2021-06-29 05:57 AM
This reply was originally posted by Jervee on APC forums on 1/12/2017
In my experience, I think that its all there is the unit can offer. Actually, you can see in the LCD Display of the unit the input and output voltage, you'll just have to manually check it in front of your unit. With regards to the NMC Slot of your unit, unfortunately, that's all there is. I wish that you'd purchased the SMT Model because even the 750VA ones has an NMC Card slot.
User | Count |
---|---|
4836 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.