Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79278members
343949posts

Writing to the Windows System Event Log using PowerChute Network Shutdown v4.2 for Window

Solved
BillP
Administrator Administrator
Administrator
0 Likes
1
71

Writing to the Windows System Event Log using PowerChute Network Shutdown v4.2 for Window

This question was originally posted by Otto on APC forums on 10/4/2016


From what I can tell PowerChute Network Shutdown v4.2 for Windows does not have the ability to write events to the Window System Event Log.  I did read that it did have that ability at one time but not any longer.

Has anyone ever come up with a way to write events to the System Event Log using some kind of script or 3rd party app?  Or is it possible to have the Network Management Card write to it independently of PCNS.  Our goal is to have Microsoft SCOM create alerts based on events.

Thanks!


Accepted Solutions
voidstar_apc
Janeway
Janeway
0 Likes
0
71

Re: Writing to the Windows System Event Log using PowerChute Network Shutdown v4.2 for Window

This was originally posted on APC forums on 10/4/2016


The NMC supports syslog, and there are syslog servers that can write to windows event logs, for example:

http://www.codeproject.com/Articles/18086/Syslog-daemon-for-Windows-Eventlog

but there are probably commercial options as well.

See Answer In Context

1 Reply 1
voidstar_apc
Janeway
Janeway
0 Likes
0
72

Re: Writing to the Windows System Event Log using PowerChute Network Shutdown v4.2 for Window

This was originally posted on APC forums on 10/4/2016


The NMC supports syslog, and there are syslog servers that can write to windows event logs, for example:

http://www.codeproject.com/Articles/18086/Syslog-daemon-for-Windows-Eventlog

but there are probably commercial options as well.