Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79139members
343564posts

Windows 10 Battery Status Icon

Solved
gamingumar_apc
Cadet
0 Likes
1
107

Windows 10 Battery Status Icon

This was originally posted on APC forums on 8/18/2019


Hi, After I installed Powerchute business edition I lost the taskbar battery status icon in Windows 10, How can I get it back?

I can only see all the info in the web portal, but I need that task bar icon too. How can I get it back?

Tags (3)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
108

Re: Windows 10 Battery Status Icon

This reply was originally posted by Bill on APC forums on 8/19/2019


Hi,

PowerChute disable the Windows battery shutdown option to prevent a conflict from occurring. If you must have the task bar icon you should uninstall PowerChute and follow the instruction in Schneider Electric FAQ FA159743 

Another option is to uninstall PowerChute and run APCUPSD as the shutdown software. It include a task bar icon. 

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
109

Re: Windows 10 Battery Status Icon

This reply was originally posted by Bill on APC forums on 8/19/2019


Hi,

PowerChute disable the Windows battery shutdown option to prevent a conflict from occurring. If you must have the task bar icon you should uninstall PowerChute and follow the instruction in Schneider Electric FAQ FA159743 

Another option is to uninstall PowerChute and run APCUPSD as the shutdown software. It include a task bar icon.