Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79193members
343731posts

Using USB to RS232 to connect SC 450VA to a QNAP

Solved
work2survive_apc
Cadet
0 Likes
1
193

Using USB to RS232 to connect SC 450VA to a QNAP

This was originally posted on APC forums on 12/4/2019


Using USB to RS232 adapter to connect SC 450VA to a QNAP?

Not sure in which section post this, my issue is the next:

My company owns a UPS 450VA which comes with a RS232 port as only communication port, and a QNAP TS-453BU-RP-4G

Does make sense to use an USB to RS232 adaptor in order to get the auto-protection running in the QNAP?
There is any other solution? Any technical spec for the Adapter?

Thanks.
APC Smart-UPS SC 450VA 230V
https://www.apc.com/shop/id/en/products/APC-Smart-UPS-SC-450VA-230V-1U-Rackmount-Tower/P-SC450RMI1U 

USB to RS232 adapter on Amazon.de
https://www.amazon.de/dp/B00QUZY4UG/ref=sr_1_3?keywords=USB+RS232&qid=1575449525&sr=8-3

UPS dialog on the QNAP
Attachments

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
193

Re: Using USB to RS232 to connect SC 450VA to a QNAP

This reply was originally posted by Bill on APC forums on 12/4/2019


Hello,

I recommend you get a UPS that offers USB support. Even with a USB to serial converter the UPS will not communicate with the USB on the QNAP. The converter cable is designed to create a serial port not convert serial to USB. 

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
194

Re: Using USB to RS232 to connect SC 450VA to a QNAP

This reply was originally posted by Bill on APC forums on 12/4/2019


Hello,

I recommend you get a UPS that offers USB support. Even with a USB to serial converter the UPS will not communicate with the USB on the QNAP. The converter cable is designed to create a serial port not convert serial to USB.