Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79503members
344311posts

Using PowerChute with a Hyperv Virtual machine with SMX1000

Solved
jeyates2_apc
Crewman
Crewman
0 Likes
1
72

Using PowerChute with a Hyperv Virtual machine with SMX1000

This was originally posted on APC forums on 8/30/2010


I have a HyperV server with 2 guest Windows 2008 OSs, connected to a SMX1000 UPS. Since Hyperv cannot monitor serial or USB ports, I had intended to run PowerChute on a Windows XP PC controlled by the same UPS. Is this the proper/best method? I set up a Command File in the XP PC to shut down the Hyperv server. The XP shut down directly from PowerChute, but the Hyperv did not. Is there a problem with credentials, or some other problem?


Accepted Solutions
jeyates2_apc
Crewman
Crewman
0 Likes
0
72

Using PowerChute with a Hyperv Virtual machine with SMX1000

This was originally posted on APC forums on 8/30/2010


I have a HyperV server with 2 guest Windows 2008 OSs, connected to a SMX1000 UPS. Since Hyperv cannot monitor serial or USB ports, I had intended to run PowerChute on a Windows XP PC controlled by the same UPS. Is this the proper/best method? I set up a Command File in the XP PC to shut down the Hyperv server. The XP shut down directly from PowerChute, but the Hyperv did not. Is there a problem with credentials, or some other problem?

See Answer In Context

1 Reply 1
jeyates2_apc
Crewman
Crewman
0 Likes
0
73

Using PowerChute with a Hyperv Virtual machine with SMX1000

This was originally posted on APC forums on 8/30/2010


I have a HyperV server with 2 guest Windows 2008 OSs, connected to a SMX1000 UPS. Since Hyperv cannot monitor serial or USB ports, I had intended to run PowerChute on a Windows XP PC controlled by the same UPS. Is this the proper/best method? I set up a Command File in the XP PC to shut down the Hyperv server. The XP shut down directly from PowerChute, but the Hyperv did not. Is there a problem with credentials, or some other problem?