Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79188members
343718posts

Upgraded to Powerchute BE 9.1.1.604,old version unistalled but still monitoring server??

Solved
BillP
Administrator Administrator
Administrator
0 Likes
1
81

Upgraded to Powerchute BE 9.1.1.604,old version unistalled but still monitoring server??

This question was originally posted by Hotmix on APC forums on 5/1/2015


Yesterday I uninstalled the Business edition Agent and Server thats shipped with the Smart-UPS X 1000 in 2012.

Server is 2008 R2 SP1.

I then installed the BE version 9.1.1.604 Server and Agent. I configured the software with the settings I required and provided a destination email address and originating email address which were different to the old version. I did not configure old version and could not log in to the software. Hence the uninstall and new install/upgrade

After a power out event overnight I discover that the old settings are being used on the server. No alerts were sent to the new settings I created yesterday and instead alerts were sent to the old settings. There is nothing common between the old settings and new.

I cannot find where those settings are, or if there is some software still on the server that is running and monitoring the UPS.

Can anyone advise what steps I can take to locate and remove these old settings please?

Thank you HMG.

Tags (1)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
81

Re: Upgraded to Powerchute BE 9.1.1.604,old version unistalled but still monitoring server??

This reply was originally posted by Bill on APC forums on 5/1/2015


Hi,

If you are only running the PowerChute Agent on 1 system then uninstall the PowerChute Server and configure the e-mail from the Agent web interface https:// :6547 All fo the setting will be stored in the agent folder - m11.cfg You do not need the Server and Console for a single Agent.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
82

Re: Upgraded to Powerchute BE 9.1.1.604,old version unistalled but still monitoring server??

This reply was originally posted by Bill on APC forums on 5/1/2015


Hi,

If you are only running the PowerChute Agent on 1 system then uninstall the PowerChute Server and configure the e-mail from the Agent web interface https:// :6547 All fo the setting will be stored in the agent folder - m11.cfg You do not need the Server and Console for a single Agent.