Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80575members
346465posts

USB to Serial adapter (Prolific) connected to Smart-UPS 1400 RM XL

Solved
OVERKILL_apc
Crewman
Crewman
0 Likes
5
155

USB to Serial adapter (Prolific) connected to Smart-UPS 1400 RM XL

This was originally posted on APC forums on 12/9/2010


I read through the other thread regarding the issues with the USB cables and the USB2.0/USB1.1 compatibility problems. There were a few posts in that thread where some people were having the same issue I'm having. And they were using a USB to RS232 adaptor with a Prolific chipset.

Server is running Windows Server 2008 x64. I've tried both the drivers that came with the adaptor, as well as the most recent ones from Prolific. And the issue persists.

Essentially:

The UPS talks to the computer without issue for somewhere in the neighbourhood of 24hrs. Around that time, it loses connectivity. A simple restart of the Agent service brings that connectivity back.

Is there a fix for this? it is a big PITA having to restart the service every morning.


Accepted Solutions
OVERKILL_apc
Crewman
Crewman
0 Likes
0
155

Re: USB to Serial adapter (Prolific) connected to Smart-UPS 1400 RM XL

This was originally posted on APC forums on 12/10/2010


Well the serial port on the server was disabled in the BIOS, and it is on the other side of the country. So not an easy thing to change. Hence the USB RS232 port.

This is the same problem as indicated by a few people in that other thread.

See Answer In Context

5 Replies 5
OVERKILL_apc
Crewman
Crewman
0 Likes
0
155

Re: USB to Serial adapter (Prolific) connected to Smart-UPS 1400 RM XL

This was originally posted on APC forums on 12/10/2010


Indeed, that is my concern. The newest version of the drivers from Prolific's website did not appear to help either.

OVERKILL_apc
Crewman
Crewman
0 Likes
0
155

Re: USB to Serial adapter (Prolific) connected to Smart-UPS 1400 RM XL

This was originally posted on APC forums on 12/9/2010


The UPS is a SmartUPS 1400 XL rack-mount.
The cable being used with the adaptor is 940-0024.

voidstar_apc
Janeway
Janeway
0 Likes
0
155

Re: USB to Serial adapter (Prolific) connected to Smart-UPS 1400 RM XL

This was originally posted on APC forums on 12/10/2010


>
The UPS talks to the computer without issue for somewhere in the neighbourhood of 24hrs. Around that time, it loses connectivity. A simple restart of the Agent service brings that connectivity back.

Is there a fix for this? it is a big PITA having to restart the service every morning.
>

It would be a bit gross but if you guys can't find a direct fix, you might try creating a batch file to [restart the service|http://technet.microsoft.com/en-us/library/cc736564%28WS.10%29.aspx] and then [schedule it to run|http://support.microsoft.com/kb/308569] every 12 hours or so.

OVERKILL_apc
Crewman
Crewman
0 Likes
0
155

Re: USB to Serial adapter (Prolific) connected to Smart-UPS 1400 RM XL

This was originally posted on APC forums on 12/10/2010


Unfortunately, one of my biggest issues with having to restart the service is that I lose my power logs/graphs. Which I find useful to monitor the utility conditions at that particular office.

OVERKILL_apc
Crewman
Crewman
0 Likes
0
156

Re: USB to Serial adapter (Prolific) connected to Smart-UPS 1400 RM XL

This was originally posted on APC forums on 12/10/2010


Well the serial port on the server was disabled in the BIOS, and it is on the other side of the country. So not an easy thing to change. Hence the USB RS232 port.

This is the same problem as indicated by a few people in that other thread.