Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80577members
346470posts

UPS for a corrosive environment?

Solved
HemeAqui_apc
Ensign
Ensign
0 Likes
4
108

UPS for a corrosive environment?

This was originally posted on APC forums on 5/21/2009


Hello,

Can you tell me if one of the following 20kVA UPS can support a corrosive, high relative humidity environment?
[SURT20KRMXLI|http://www.apc.com/resource/include/techspec_index.cfm?base_sku=SURT20KRMXLI&total_watts=50&ISOCount...]
[SUVTP20KH3B4|http://www.apc.com/resource/include/techspec_index.cfm?base_sku=SUVTP20KH3B4&total_watts=4000&ISOCou...]

Or maybe a MGE Galaxy (20kVA, three phase 380Vac, 400Vac)

Thanks,

HA


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
108

Re: UPS for a corrosive environment?

This reply was originally posted by Angela on APC forums on 5/21/2009


is there a certain standard that this pertains to? like a UL standard?

See Answer In Context

4 Replies 4
HemeAqui_apc
Ensign
Ensign
0 Likes
0
108

Re: UPS for a corrosive environment?

This was originally posted on APC forums on 5/22/2009


Hi,

Actually yes, it is required UL certification but I'm not sure if the UL certification is enough to assure that the UPS can support hostile (corrosive) environment.

Greetings,

HA

BillP
Administrator Administrator
Administrator
0 Likes
0
108

Re: UPS for a corrosive environment?

This reply was originally posted by Angela on APC forums on 5/25/2009


i just meant to ask if you know that a piece of equipment that can be put in a corrosive environment pertains to a certain standard so then i could see if any of APC's UPS meet that standard.

all of the UPSs are UL 1449 rated i believe but there are other standards like UL509a for instance which pertains to outdoor use, etc..maybe this type of environment has a standard that goes along with it?

HemeAqui_apc
Ensign
Ensign
0 Likes
0
108

Re: UPS for a corrosive environment?

This was originally posted on APC forums on 5/27/2009


Hi,

Well that info I don't know (what other equipment will be there). Thanks for the help.

HA

BillP
Administrator Administrator
Administrator
0 Likes
0
109

Re: UPS for a corrosive environment?

This reply was originally posted by Angela on APC forums on 5/21/2009


is there a certain standard that this pertains to? like a UL standard?