Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-28 04:30 AM
This was originally posted on APC forums on 4/6/2016
Hi There,
We have plugged in USB Cable from APC USB UPS to server and we can see it installed in Device Manager as shown in Image below.
But when we are trying to Add the device to APC PowerChute Business Edition Deluxe Software it is not showing that Device.
Can I please get some suggestion re this.
Thanks,
Jatin
Posted: 2021-06-28 04:30 AM
This reply was originally posted by Gareth on APC forums on 4/13/2016
I think the HID UPS Battery in the device manager should update to an APC version with the software, you may be able to right click and update manually, then untick the show compatible hardware to see if the APC option is there, click that and then powerchute will detect it.
Posted: 2021-06-28 04:30 AM
This reply was originally posted by Bill on APC forums on 4/7/2016
Hi,
Is the UPS not being discovered by the PowerChute Server and Console or is the UPS not being discovered when you attempt to install the PowerChute Agent? Also, What model Smart-UPS are you attempting to communicate with?
Posted: 2021-06-28 04:30 AM
This was originally posted on APC forums on 4/7/2016
Hi Bill,
Yes it is not getting discovered by the server and console.
Model: APC Smart-Ups 750
Thanks,
Jatin
Posted: 2021-06-28 04:30 AM
This reply was originally posted by Bill on APC forums on 4/11/2016
Hi,
Can you log into the PowerChute Agent web interface and if so does the web interface show that the UPS and the Agent are communicating? To log into the Agent web interface open a web browser (Internet Explore, Firefox, Chrome) and enter https://
Posted: 2021-06-28 04:30 AM
This reply was originally posted by Bill on APC forums on 4/12/2016
Hi,
The PowerChute Server is not discovering the Agent because there is a communication error between the Agent and the UPS. What is the model and Serial numbers of the UPS and what version of PowerChute Agent, Server, and Console are installed? Also, What communications cable is attached between the UPS and computer?
Posted: 2021-06-28 04:30 AM
This was originally posted on APC forums on 4/12/2016
Hi Bill,
Details as below:
Thanks,
Jatin
Posted: 2021-06-28 04:30 AM
This reply was originally posted by Bill on APC forums on 4/13/2016
Hi,
Uninstall the PowerChute Agent and then reinstall. When installing verify that the UPS is discovered by the installer. Once the Agent is reinstall log into the Agent web interface to verify communication is established. If communication has been established open the Console and add the Agent to the PowerChute Server.
NOTE: When installing the Agent be sure to use the same user name and password and used with the PowerChute Server.
Posted: 2021-06-28 04:30 AM
This reply was originally posted by Gareth on APC forums on 4/13/2016
I think the HID UPS Battery in the device manager should update to an APC version with the software, you may be able to right click and update manually, then untick the show compatible hardware to see if the APC option is there, click that and then powerchute will detect it.
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.