Hello,
I did have some problem with the shutdown signal from NMC3 and servers.
My servers are getting power from SRT5KXLI with built in NMC3. They are configured to wait until low battery before safe shutdown.
A couple of days ago, UPS detected "UPS: Bypass not in range ; distorted waveform" and UPS started feeding the devices from the battery due to this.
However, my servers went immediately to the safe shutdown without waiting for "low battery". Later on when I tried to reproduce the issue by cutting the input power of the UPS, servers were still on as should be since UPS battery was full.
I would like to ask when UPS detects distorted waveform, does it send shutdown signal through SNMP?
Furthermore, how can I simulate a distorted waveform so that I can debug this issue?
Some details:
Green mode is disabled and UPS is on online mode.
Network firmware: v1.5.1.1
Model number: 0N-1557
Hardware Revision: 3
Thanks in advance