Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-30 11:09 PM
This was originally posted on APC forums on 11/26/2015
OK, so we have an installed LX which is down to it's last power module, and by chance I got offered another Symmetra really cheap as someone I know was closing down due to bad health.
Now firstly, I'm confused as to which is the older unit - I assume the Symmetra we've just bought, with "plastic" battery packs (SYBATT) and plastic rails on the bottom of the PMs (SYPM), rather than the LX we have installed with metal battery packs (SYBT5) and no plastic runners on the bottom of the power modules (SYPM4KI). I don't really care as the one we've just got has enough PMs to do us with +1 redundancy.
But we have a battery expansion cab (Xr frame) on the LX. The batteries seem to be the same voltage, and the replacement Symmetra has a comms card in the back for talking to an XR frame. Does anyone know if the two systems are compatible for that ?
Also, while the PMs are different, they aren't that different. The LX module is slightly longer overall, but slightly shorter at the back where the air vent is, but the connectors appear to be identical. Well I suppose the worst that can happen is it goes bang if I try it
Posted: 2021-06-30 11:09 PM
This reply was originally posted by Angela on APC forums on 11/30/2015
Hello,
Symmetra Power Array (the beige one) has been discontinued for about 10 years now which is when Symmetra LX was introduced. The LX is still current. There are no modules that are compatible between them.
The exception is external battery cabinets. Here is a link to the model compatibility -> http://www.apc.com/support/index?page=content&country=ITB〈=en&locale=en_US&id=FA157425
You'll have to check the model on the external cabinet itself and see what you have.
Posted: 2021-06-30 11:09 PM
This reply was originally posted by Angela on APC forums on 11/30/2015
Hello,
Symmetra Power Array (the beige one) has been discontinued for about 10 years now which is when Symmetra LX was introduced. The LX is still current. There are no modules that are compatible between them.
The exception is external battery cabinets. Here is a link to the model compatibility -> http://www.apc.com/support/index?page=content&country=ITB〈=en&locale=en_US&id=FA157425
You'll have to check the model on the external cabinet itself and see what you have.
User | Count |
---|---|
4834 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.