Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-30 08:55 PM
This was originally posted on APC forums on 5/21/2011
Ok I'm having some problems in getting this to work properly and after searching the forums I haven't had much luck so far in finding a solution. I have a BackUPS Pro 1100 which came with a standard serial cable. Unfortunately my PC does not have a serial connection so I couldn't hook it straight in, however I do have a USB to Serial converter which I was able to get drivers for and Windows shows as working properly. The problem is that for some reason the Agent software will not detect the UPS at all. I should note that if I try and open it via putty with it set to COM2 2400-8-1-None-None all I have happen is to have the windows alert sound play.
Edit After re-reading my post I think I was a bit short on the information. I'm trying to use PowerChute Business Edition v9 on my Windows 7 64 bit system. The serial cable that I'm using is the serial cable that came boxed with the UPS.
Message was edited by: cpatricca
Posted: 2021-06-30 08:56 PM
This was originally posted on APC forums on 5/28/2011
Jon,
I don't see a model number anywhere on the cable that came with the UPS in the package but from what I read in the manual it's the basic signalling cable and doesn't send SMART signals. I did try setting it manually to use the COM port I had assigned to the USB to serial adapter and set it to use basic signalling. I still couldn't get it to communicate with the agent on the PC it's hooked up to.
Posted: 2021-06-30 08:56 PM
This reply was originally posted by Jonathan on APC forums on 5/23/2011
Hello Chris,
Can you provide the exact model number of the cable that came with the UPS. Also, when you installed PCBE did you used the auto detect features? Since you are using an old BackUPS Pro, it might work with PCBE but you need to manually configure it and used Simple Signaling.
Posted: 2021-06-30 08:56 PM
This was originally posted on APC forums on 5/28/2011
Jon,
I don't see a model number anywhere on the cable that came with the UPS in the package but from what I read in the manual it's the basic signalling cable and doesn't send SMART signals. I did try setting it manually to use the COM port I had assigned to the USB to serial adapter and set it to use basic signalling. I still couldn't get it to communicate with the agent on the PC it's hooked up to.
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.