Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-28 04:33 AM
This was originally posted on APC forums on 4/13/2016
Will the internals of a SU700RM2U work with the four-battery tray from a SU1400RM2U? Seems to me they both operate at 24V and the extra batteries "should" only require runtime recalibration at most--but I'm not willing to bet my 700 on that without some corroboration.
Posted: 2021-06-28 04:33 AM
This was originally posted on APC forums on 4/14/2016
I haven't tried it myself, but I see no obvious reason why it wouldn't work. (You might have to configure the unit to believe it has a externally attached battery to get the calibrations right.) I do plan to try it, if I can get the four battery tray at a reasonable cost. Or I could probably add the wiring to what I've got already...if I find the time.
You may also want to install a cooling fan. I believe the SU700RM2U will overheat quickly under anything more than 50% load if the runtime is extended. I plan to add one to mine as a matter of course.
Posted: 2021-06-28 04:33 AM
This was originally posted on APC forums on 4/14/2016
I haven't tried it myself, but I see no obvious reason why it wouldn't work. (You might have to configure the unit to believe it has a externally attached battery to get the calibrations right.) I do plan to try it, if I can get the four battery tray at a reasonable cost. Or I could probably add the wiring to what I've got already...if I find the time.
You may also want to install a cooling fan. I believe the SU700RM2U will overheat quickly under anything more than 50% load if the runtime is extended. I plan to add one to mine as a matter of course.
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.