Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-30 08:12 PM
This was originally posted on APC forums on 1/11/2017
The SMC1500 (SAU1500 -- serial ASO-129330095) hasn't been used for at least 10 years.
With the batteries in and plugged into power, the UPS chirps and the lights continually flash in no apparent order. I created a YouTube video with what it looks like.
Without the batteries connected and plugged into power, the UPS doesn't chirp or light.
Here's are more details:
Any ideas? Or is the UPS ready for a trip to the recycling center?
Posted: 2021-06-30 08:13 PM
This was originally posted on APC forums on 1/15/2017
William,
Let's chat offline. Contact me at stevebass@gmail.com
--Steve
I
Posted: 2021-06-30 08:12 PM
This reply was originally posted by Jonathan on APC forums on 1/11/2017
Hi Steve,
Unfortunately, the UPS is already dead but you can still use it for our TradeUPS program. You will get a new UPS at a discounted price.
Posted: 2021-06-30 08:12 PM
This was originally posted on APC forums on 1/11/2017
I'm a tinkerer and get a kick out of fixing dead things. Unfortunately, I've never worked on a UPS. Any hints on what may be malfunctioning?
Also: which new model would use the 2 RBC7 batteries?
Thanks
Posted: 2021-06-30 08:12 PM
This was originally posted on APC forums on 1/13/2017
Did you press and hold the power button for a few sec. until you heard it crip and then release it.
this is called doing a cold start...
Posted: 2021-06-30 08:13 PM
This was originally posted on APC forums on 1/13/2017
Thanks for the suggestion, John. I tried that. Didn't help.
Posted: 2021-06-30 08:13 PM
This was originally posted on APC forums on 1/14/2017
It possible that you can install a (cheap) network management card - (an AP9617 on ebay) and see if it will power up - the yellow light will come on if it has power. With the latest NMC firmware, you may be able to get some error codes that lead you in the right direction for a repair - or potentially upgrade the UPS firmware. There are a few wiring schemas on the web for the older models (SU/SUA) that if you have electronics skills, may be able to repair. DANGER - HIGH VOLTAGES ABOUND!
Posted: 2021-06-30 08:13 PM
This was originally posted on APC forums on 1/14/2017
Hey Mark, thanks for your suggestion. But I think your nice and bright warning pushed me into thinking how much more fun it'd be to enjoy my low-risk geocaching hobby or maybe tend to the lettuce in my garden.
Seriously, I'm putting an ad on Craigslist or freecycle and offering it up as a freebie for someone else to tinker. Unless, of course, you want it (and in this case, "batteries included"!).
Posted: 2021-06-30 08:13 PM
This was originally posted on APC forums on 1/14/2017
It looks to me like there's a possible short circuit in whatever portion of the power supply feeds the low voltage electronics (microcontroller, etc.). This could explain the "pulsating" behavior -- the circuit starts up, hits a built in current limit (or the limits of the components) and shuts down to protect itself. Only there's no "latch" to keep it shut down, so it repeats forevermore.
These units are famous for developing bad capacitors. As best I remember, it is the 22uF capacitors that are the trouble makers. There might be others.
I might be interested in the unit, if you decide to get rid of it.
Posted: 2021-06-30 08:13 PM
This was originally posted on APC forums on 1/15/2017
William,
Let's chat offline. Contact me at stevebass@gmail.com
--Steve
I
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.