Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79357members
344053posts

SmartUPS 1500 chirps and flashes -- but doesn't work

Solved
stevebass_apc
Crewman
Crewman
0 Likes
8
244

SmartUPS 1500 chirps and flashes -- but doesn't work

This was originally posted on APC forums on 1/11/2017


The SMC1500 (SAU1500 -- serial ASO-129330095) hasn't been used for at least 10 years.

With the batteries in and plugged into power, the UPS chirps and the lights continually flash in no apparent order. I created a YouTube video with what it looks like.

Without the batteries connected and plugged into power, the UPS doesn't chirp or light.

Here's are more details:

  • Neither button -- on/test and off -- stops the chirping or flashing.
  • The batteries are fine, terminals are clean, and the wiring is correct. I recharged then from a vehicle battery charger and tested with a voltmeter. They're holding a charge.
  • The fuse appears good -- I can see the copper wire across the window.
  • The  circuit breaker hasn't popped up.
  • I tested the UPS at different power outlets. A light bulb doesn't work on any of the UPS outlets with the batteries or if the UPS is just connected to power.
  • It has never been connected to the PowerChute app.
  • The braindead technique hasn't helped.

Any ideas? Or is the UPS ready for a trip to the recycling center?


Accepted Solutions
stevebass_apc
Crewman
Crewman
0 Likes
0
244

Re: SmartUPS 1500 chirps and flashes -- but doesn't work

This was originally posted on APC forums on 1/15/2017


William,

Let's chat offline. Contact me at stevebass@gmail.com

--Steve

I

See Answer In Context

8 Replies 8
BillP
Administrator Administrator
Administrator
0 Likes
0
244

Re: SmartUPS 1500 chirps and flashes -- but doesn't work

This reply was originally posted by Jonathan on APC forums on 1/11/2017


Hi Steve,

Unfortunately, the UPS is already dead but you can still use it for our TradeUPS program. You will get a new UPS at a discounted price.

stevebass_apc
Crewman
Crewman
0 Likes
0
244

Re: SmartUPS 1500 chirps and flashes -- but doesn't work

This was originally posted on APC forums on 1/11/2017


I'm a tinkerer and get a kick out of fixing dead things. Unfortunately, I've never worked on a UPS. Any hints on what may be malfunctioning?

Also: which new model would use the 2 RBC7 batteries?

Thanks

jeb1969_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
244

Re: SmartUPS 1500 chirps and flashes -- but doesn't work

This was originally posted on APC forums on 1/13/2017


Did you press and hold the power button for a few sec. until you heard it crip and then release it.

this is called doing a cold start...

stevebass_apc
Crewman
Crewman
0 Likes
0
244

Re: SmartUPS 1500 chirps and flashes -- but doesn't work

This was originally posted on APC forums on 1/13/2017


Thanks for the suggestion, John. I tried that. Didn't help.

MarkC_apc
Commander
Commander
0 Likes
0
244

Re: SmartUPS 1500 chirps and flashes -- but doesn't work

This was originally posted on APC forums on 1/14/2017


It possible that you can install a (cheap) network management card - (an AP9617 on ebay) and see if it will power up - the yellow light will come on if it has power.  With the latest NMC firmware, you may be able to get some error codes that lead you in the right direction for a repair - or potentially upgrade the UPS firmware.  There are a few wiring schemas on the web for the older models (SU/SUA) that if you have electronics skills, may be able to repair.  DANGER - HIGH VOLTAGES ABOUND!

stevebass_apc
Crewman
Crewman
0 Likes
0
244

Re: SmartUPS 1500 chirps and flashes -- but doesn't work

This was originally posted on APC forums on 1/14/2017


Hey Mark, thanks for your suggestion. But I think your nice and bright warning pushed me into thinking how much more fun it'd be to enjoy my low-risk geocaching hobby or maybe tend to the lettuce in my garden.

Seriously, I'm putting an ad on Craigslist or freecycle and offering it up as a freebie for someone else to tinker. Unless, of course, you want it (and in this case, "batteries included"!).

UnexpectedBill_apc
Captain
Captain
0 Likes
0
244

Re: SmartUPS 1500 chirps and flashes -- but doesn't work

This was originally posted on APC forums on 1/14/2017


It looks to me like there's a possible short circuit in whatever portion of the power supply feeds the low voltage electronics (microcontroller, etc.). This could explain the "pulsating" behavior -- the circuit starts up, hits a built in current limit (or the limits of the components) and shuts down to protect itself. Only there's no "latch" to keep it shut down, so it repeats forevermore.

These units are famous for developing bad capacitors. As best I remember, it is the 22uF capacitors that are the trouble makers. There might be others.

I might be interested in the unit, if you decide to get rid of it.

stevebass_apc
Crewman
Crewman
0 Likes
0
245

Re: SmartUPS 1500 chirps and flashes -- but doesn't work

This was originally posted on APC forums on 1/15/2017


William,

Let's chat offline. Contact me at stevebass@gmail.com

--Steve

I