This was originally posted on APC forums on 11/29/2016
Above UPS which was installed around May/June 2015 started to go into bypass mode some days ago. Other times I find unit completely off in the morning and have to switch on manually. From event logs i see above message, also noted UPS logs are saying charger overvoltage. Details of unit below:
Model: |
Smart-UPS SRT 10000 |
SKU: |
SRT10KXLI |
Serial Number: |
QS1422171400 |
Firmware Revision: |
UPS 01.4 (ID1002) |
Manufacture Date: |
05/31/2014 |
Apparent Power Rating: |
10000 VA |
Real Power Rating: |
10000 W |
Battery SKU: |
APCRBC140 |
|
|
UPS Fault Logs |
Number | Time (ms) | Event Code | Event |
1 |
56053457168 |
149 |
Charger Overvoltage |
2 |
55868156033 |
192 |
|
3 |
218882320 |
154 |
Interprocessor Communications Fault |
4 |
32061922048 |
192 |
|
5 |
55868156033 |
149 |
Charger Overvoltage |
6 |
55868156033 |
192 |
|
7 |
43402692124 |
149 |
Charger Overvoltage |
8 |
55868156033 |
192 |
|
9 |
1033459751968 |
149 |
Charger Overvoltage |
10 |
983916609536 |
149 |
Charger Overvoltage |
|
Attached event and debug logs.