Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80824members
346893posts

Smart-UPS SMT750 PCBE 9 Data Log "No Data Logged'

Solved
drcastillo_apc
Crewman
Crewman
0 Likes
2
116

Smart-UPS SMT750 PCBE 9 Data Log "No Data Logged'

This was originally posted on APC forums on 10/27/2012


Everything thing works inside the web agaent except can't get it to create the datalog so I can monitor the data.
I have enabled data logging.
Windows 7 64Bit
Have tried both versions of PCBE 9.0.0.13 and 9.0.1. rebooting and cleaning registry with ccleaner in between uninstall and reinstall of older version.
Have to use the USB cable as this computer does not have a serial port.
There is a eventlog file but no datalog file.
Tried creating a datalog file and added to the C:\Program Files (x86)\APC\PowerChute Business Edition\agent folder but as soon as I start the agent it deletes the datalog file.
Have disabled MS Security Essentials, no other virus\malware software installed.
This is a fresh install of Windows.
I have another computer with a Smart-UPS 1500 running PCBE 9.0.1 with Windows 7 64Bit using the USB cable and it creates the datalog file and I can view the data fine.

Does anyone have any ideas?

Thanks,
David


Accepted Solutions
drcastillo_apc
Crewman
Crewman
0 Likes
0
116

Re: Smart-UPS SMT750 PCBE 9 Data Log "No Data Logged'

This was originally posted on APC forums on 10/30/2012


Just recieved an email from Bill Pasquill from schneider-electric.
Hopefully I can help troubleshoot this.
Thanks,
David

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
116

Re: Smart-UPS SMT750 PCBE 9 Data Log "No Data Logged'

This reply was originally posted by Angela on APC forums on 10/29/2012


this is an issue we have seen before unfortunately and we are still looking at the root cause. i will have someone contact you directly in order to further debug the issue if that is alright.

drcastillo_apc
Crewman
Crewman
0 Likes
0
117

Re: Smart-UPS SMT750 PCBE 9 Data Log "No Data Logged'

This was originally posted on APC forums on 10/30/2012


Just recieved an email from Bill Pasquill from schneider-electric.
Hopefully I can help troubleshoot this.
Thanks,
David