Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-28 09:34 PM
This was originally posted on APC forums on 3/14/2009
I picked up a used Smart-UPS 750 from a company that was getting rid of it. They said that it didn't work. I still took it home optimistically hoping to use it on my computer at home (I thought that it might be a simple fix like buying a replacement battery). First things first; I'm new to this kind of UPS, and therefore I have several questions.
First - The UPS does not power on. No lights, no sound, nothing at all. I decided to pull out off the front cover and have a look inside. The battery looks great... In fact, the whole unit looks almost like new. I got out a multimeter and tested for continuity of the wires. The two middle wires connected fine. The two outside wires did not. Is this normal?
Second - On the back is a big plastic cover with the words under it "Battery Connector". I thought that all of the battery backup was handled inside the unit. I tried to open it up and couldn't. What is this used for? Do I have to use it? How am I supposed to open it up?
Third - Seeing that this is some kind of server UPS, would it work for a personal computer setup?
Is the entire UPS shot or is it just the battery?
~Chris
Posted: 2021-06-28 09:34 PM
This reply was originally posted by Tim on APC forums on 3/16/2009
You would want to take a measurement off the connector used to connect the battery to the UPS itself.
Posted: 2021-06-28 09:34 PM
This reply was originally posted by Angela on APC forums on 3/14/2009
Posted: 2021-06-28 09:34 PM
This was originally posted on APC forums on 3/14/2009
Here is a diagram of my battery (actually it's two batteries):
Edit: Couldn't get my diagram to show up right.
I've ordered it like this:
1 - 3 - 4 - 2
1 and 4 are negative. 3 and 2 are positive.
1 is connected to 2 and 3 is connected to 4. When testing for continuity, 3 and 4 connect, but 1 and 2 do not. 1 and 2 lead to a connector seems to just slide into the UPS. 3 and 4 must connect the two batteries together.
Which set am I supposed to check the voltage with? Shouldn't both sets of wires make a circuit?
~Chris
Message was edited by: geeked
Message was edited by: geeked
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.