APC UPS Data Center & Enterprise Solutions Forum
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-30 07:19 AM . Last Modified: 2024-03-07 11:13 PM
I had this unit for five years now. I always replaced batteries with genuine APC at least two times: not a single issue.
Recently, I have removed the UPS for scheduled maint, cleaned the ventilation holes and then put it back but without connecting any load. When I turned on the device, it performed a self-test which was not successful. The display showed a fault red light and the message: "fault state: output over volt". By attaching all the load back, and cycling the UPS power OFF-ON, the self-test was successfully passed. The load was 12% (120W).
If I attach something lower than 120W, the UPS won't pass the self-test neither is able to provide UPS protection to the outlets if the AC cable is removed (batteries fully charged).
Question #1:
Is there a Minimum load under which the UPS can't operate?
Question #2:
It is normal to get the "fault state: output over volt" without load?
I suspect a system malfunction because other UPS I have installed (different maker) are able to work and perform a self-test with no load attached. In this case, is there something I could do to verify the device?
Thank you very much,
Adam.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-30 07:19 AM . Last Modified: 2024-03-07 11:13 PM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-30 07:19 AM . Last Modified: 2024-03-07 11:13 PM
After nearly two months, no answer!
Anyone?
Thank you,
AH
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.