Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-30 06:09 AM
This was originally posted on APC forums on 2/17/2008
I just purchased two used Smart-UPS 1400s, which utilize a serial connection. When I connect the serial cable to my server, then plug it into the UPS, it immediately kills the power to the UPS and thus, my server.
I assumed they use a standard db9 RS232 connection. Is that not right?
I tried this with and without having PowerChute installed. It made no difference.
When the serial cable was attached at both ends, I could not even turn the UPS on. I had to disconnect the cable from the UPS in order to power everything back up.
Any advice and insight would be much appreciated.
tia.
Posted: 2021-06-30 06:09 AM
This was originally posted on APC forums on 2/19/2008
Posted: 2021-06-30 06:09 AM
This reply was originally posted by Annie on APC forums on 2/17/2008
Hey,
You need to use the cable shipped with the UPS. Its part number should be 940-0024C or 940-0024D, or 940-1524C or 940-1524D , this depends on what specific UPS model you are using.
Posted: 2021-06-30 06:09 AM
This was originally posted on APC forums on 2/18/2008
Thanks for the reply.
As I purchased them used, they didn't come with cables. I'll see if I can find some.
Todd.
Posted: 2021-06-30 06:09 AM
This was originally posted on APC forums on 2/19/2008
User | Count |
---|---|
4836 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.