Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-07-09 01:11 AM
This was originally posted on APC forums on 11/28/2019
HI,
I want to to use the uninstall built into powerchute to remove the software. I found the string:
"C:\Program Files (x86)\InstallShield Installation Information\{BCE9F441-9027-4911-82E0-5FB28057897D}\setup.exe" -runfromtemp -l0x0409 AnyText -removeonly"
which is also contained inside the uninstall.cmd file. However the dang things keeps prompting to confirm the removal of all the software.
Does anyone know the switch to let it continue silently?
Thanks in advance
Posted: 2021-07-09 01:12 AM
This reply was originally posted by Bill on APC forums on 12/13/2019
Hi,
It's up to you as they will not hurt anything if they remain. I have cleaned them up using CCleaner but that is not a silent app.
One other thing I forgot to include earlier is when PowerChute is installed it opens ports in the firewall. If you would to remove the rules the command is netsh advfirewall firewall delete rull name= "PowerChute Business Edition Agent".
Posted: 2021-07-09 01:11 AM
This reply was originally posted by Bill on APC forums on 12/2/2019
Hello,
Are you attempting to uninstall PCPE or PCBE and what version of PowerChute are you attempting to uninstall?
Posted: 2021-07-09 01:11 AM
This was originally posted on APC forums on 12/2/2019
Hi Bill, PCBE, Thanks Gary
Posted: 2021-07-09 01:11 AM
This reply was originally posted by Bill on APC forums on 12/3/2019
Hi,
We do not offer silent uninstall of PCBE however you can create a batch script to do so. I have attached a text file that when change to a .cmd will remove PCBE Agent from 64 bit system. The command file has been tested with PCBE Agents 9.2.1, 9.5, and 10.0.
If you need to remove from 32 bit system the registry entries are list in Schneider Electric FAQ FA159894
Posted: 2021-07-09 01:11 AM
This was originally posted on APC forums on 12/4/2019
thanks Bill.
Posted: 2021-07-09 01:12 AM
This was originally posted on APC forums on 12/12/2019
Hi Bill,
In the registry there are a whole heap of shared DLL's which point to the APC folder. All the shared DLL's are for JRE, do these need to be cleaned up as well, is it likely to break something else which use
Gary
Posted: 2021-07-09 01:12 AM
This reply was originally posted by Bill on APC forums on 12/13/2019
Hi,
It's up to you as they will not hurt anything if they remain. I have cleaned them up using CCleaner but that is not a silent app.
One other thing I forgot to include earlier is when PowerChute is installed it opens ports in the firewall. If you would to remove the rules the command is netsh advfirewall firewall delete rull name= "PowerChute Business Edition Agent".
User | Count |
---|---|
4836 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.