Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
Should UPS Output be treated as a Separately Derived System per NEC?
APC UPS Data Center & Enterprise Solutions Forum
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-06-2806:06 AM. Last Modified: 2024-03-1802:46 AM
Should UPS Output be treated as a Separately Derived System per NEC?
Installing a 15 kVA UPS, 208 V, 3-phase input; 208Y/120, 3-phase, 4-wire wye out (SUVTR20KF4B5S plus Battery Cabinets). The manual does not specifically state, but wouldn't NEC consider the UPS Output a "Separately Derived System" and be treated much like the secondary of a new 15 kVA xfmr? Specifically, shouldn't the new UPS installation require an additional Grounding Electrode Conductor (GEC)? Note that I'm NOT asking about an Equipment Grounding Conductor (which would be typically be installed with the supply & load conductors). I'm asking about a "Grounding Electrode Conductor" similar to that installed between a transformer neutral to building steel and/or water piping.