Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79283members
343958posts

Set number of connected batteries using AP9631 NMC card.

Solved
wgstarks_apc
Crewman
Crewman
0 Likes
2
107

Set number of connected batteries using AP9631 NMC card.

This was originally posted on APC forums on 8/15/2016


I have an SURTA1500RMXL2U UPS with a connected SURTA48RMXLBP2U external battery pack. I need to change the number of batteries in the ups settings via the installed NMC card (AP9631). I've set her through the command line guide but I don't see what command to use to configure this setting.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
107

Re: Set number of connected batteries using AP9631 NMC card.

This reply was originally posted by Angela on APC forums on 8/15/2016


Right, I do not see an option for this on the command line for type of UPS when I checked. We'll have to fix those other issues up first and then we'll hopefully be able to take care of it. 

See Answer In Context

2 Replies 2
wgstarks_apc
Crewman
Crewman
0 Likes
0
107

Re: Set number of connected batteries using AP9631 NMC card.

This was originally posted on APC forums on 8/15/2016


So I'm guessing this can't be set from the command line? Hopefully I'll be able to get the web interface working. Thanks for your help with these issues.

BillP
Administrator Administrator
Administrator
0 Likes
0
108

Re: Set number of connected batteries using AP9631 NMC card.

This reply was originally posted by Angela on APC forums on 8/15/2016


Right, I do not see an option for this on the command line for type of UPS when I checked. We'll have to fix those other issues up first and then we'll hopefully be able to take care of it.