Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-29 04:50 AM
This was originally posted on APC forums on 8/15/2016
I have an SURTA1500RMXL2U UPS with a connected SURTA48RMXLBP2U external battery pack. I need to change the number of batteries in the ups settings via the installed NMC card (AP9631). I've set her through the command line guide but I don't see what command to use to configure this setting.
Posted: 2021-06-29 04:51 AM
This reply was originally posted by Angela on APC forums on 8/15/2016
Right, I do not see an option for this on the command line for type of UPS when I checked. We'll have to fix those other issues up first and then we'll hopefully be able to take care of it.
Posted: 2021-06-29 04:51 AM
This was originally posted on APC forums on 8/15/2016
So I'm guessing this can't be set from the command line? Hopefully I'll be able to get the web interface working. Thanks for your help with these issues.
Posted: 2021-06-29 04:51 AM
This reply was originally posted by Angela on APC forums on 8/15/2016
Right, I do not see an option for this on the command line for type of UPS when I checked. We'll have to fix those other issues up first and then we'll hopefully be able to take care of it.
User | Count |
---|---|
4834 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.