Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79320members
344001posts

Server startup after Shutdown

Solved
craigoasis_apc
Crewman
Crewman
0 Likes
4
212

Server startup after Shutdown

This was originally posted on APC forums on 6/18/2015


Hi,

I have various Smart UPS's installed at clients, ive been sold to that these UPS's, can issue a clean shutdown command to the servers thru powerchute, then the servers shutdown all OK.

Then when the power is restored after sometime, even after the UPS is drained flat.. It will then start the server up, i cannot seem to get this to work. I believe its actually impossible.

How does the APC issue a command to an off server to startup.

Can anyone shed some light on this?

Thanks in advnace.


Accepted Solutions
voidstar_apc
Janeway
Janeway
0 Likes
0
213

Re: Server startup after Shutdown

This was originally posted on APC forums on 6/19/2015


There should be a BIOS setting to turn the computer back on after a power outage. There's a picture here:

http://www.servethehome.com/keeping-servers-bios-setup-availibility/

See Answer In Context

4 Replies 4
BillP
Administrator Administrator
Administrator
0 Likes
0
213

Re: Server startup after Shutdown

This reply was originally posted by Bill on APC forums on 6/18/2015


Craig,

the UPS cannot issue a power on command that is done through the BIOS of the computer. See Kbase FA159547.

craigoasis_apc
Crewman
Crewman
0 Likes
0
213

Re: Server startup after Shutdown

This was originally posted on APC forums on 6/18/2015


Thanks Bill,

will the BIOS setting assist even if powerchute has told  the server to shutdown?

BillP
Administrator Administrator
Administrator
0 Likes
0
213

Re: Server startup after Shutdown

This reply was originally posted by Bill on APC forums on 6/18/2015


Craig,

Yes. If set up properly configured when PowerChute commands the OS down the UPS will wait a defined amount of time than then kill power to the outlets. When AC is restored the UPS will restore power to the outlets which in turn causes the computer to start up.

voidstar_apc
Janeway
Janeway
0 Likes
0
214

Re: Server startup after Shutdown

This was originally posted on APC forums on 6/19/2015


There should be a BIOS setting to turn the computer back on after a power outage. There's a picture here:

http://www.servethehome.com/keeping-servers-bios-setup-availibility/