Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79160members
343633posts

Serial Communication with APC UPS RM 750 (SMT750RMI2U)

Solved
esekh_apc
Crewman
Crewman
0 Likes
4
333

Serial Communication with APC UPS RM 750 (SMT750RMI2U)

This was originally posted on APC forums on 2/28/2017


Try connect to  APC UPS  RM 750 (SMT750RMI2U) via serial interface and cable that was with device 940-625A. Used real COM1 port where OK work early old my UPS SMART 1000.

I try to use software:

  • PowerChute Business 9.2.
  • APCUPSD
  • PLINK for direct connect to com1

But device not detected. COM Port not answer.

By post :

http://forums.apc.com/spaces/5/smart-ups-symmetra-lx-rm/forums/general/12876/serial-communication-wi...

I have information that SMT750 should work with serial port in any case.

When i test to use with USB  connection  PowerChute  Business  9.2 detect ups OK .

I manual described that can work or serial or USB  connection in one time. May be need switch by some procedure ? 

Factory reset not help in my case.

SN: AS1621241318

Tags (3)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
333

Re: Serial Communication with APC UPS RM 750 (SMT750RMI2U)

This reply was originally posted by Bill on APC forums on 5/22/2019


Hello,

What software are you trying to connect to the the UPS over serial comm? If anything other than PowerChute Business Edition it is not supported. If PowerChute Business Edition is failing to discover the UPS over serial comm what version of PowerChute are you installing? 

See Answer In Context

4 Replies 4
esekh_apc
Crewman
Crewman
0 Likes
0
333

Re: Serial Communication with APC UPS RM 750 (SMT750RMI2U)

This was originally posted on APC forums on 3/3/2017


Thanks for SerialTerm.exe. By this apps I detected wrong MB cable connector. They was with other order of pins.
And now I know that new SMART-UPS use SPEED 9600.8.n.1.n,  with old SMART-UPS used speed 2400.8.n.1.n

At image show order of pins.

But now other problem with start Agent.

After many reinstall of program agent 9.2, now not started service of PowerChute Business Edition Agent.

7024 Error Microsoft-Windows-Service Control Manager System 03.03.2017 4:20:05

The APC PBE Agent service terminated with the following service-specific error: The operation completed successfully.

101 Error APCPBEAgent Application 03.03.2017 4:20:04

Error: 0, Time out 90 seconds. Service start operation canceled.

But early at this host agent started correctly.

It  link not resolve same problem.

Server Core HV-2016. USB connection. APC UPS RM 750.

Logs: pcbe.log

2017-03-02 19:41:26,108 [main] INFO - [application.PicardApplication] - Legacy logging adapter enabled.
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] Java Runtime: Java(TM) SE Runtime Environment (ve
rsion: 1.8.0_31)
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] Java Home: C:\PROGRA~2\APC\POWERC~1\JRE18~1.0_3
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] JVM: Java HotSpot(TM) Client VM (version: 25.31-b
07)
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] OS: Windows Server 2012 (x86)
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] Time Zone: Europe/Helsinki
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] PCBE dir: C:\PROGRA~2\APC\POWERC~1\agent
2017-03-02 19:41:26,124 [main] ERROR - [application.PicardApplication] Can not read M11.cfg file:
java.io.FileNotFoundException: m11.cfg (The system cannot find the file specified)
at java.io.FileInputStream.open(Native Method)
at java.io.FileInputStream.(Unknown Source)
at java.io.FileInputStream.(Unknown Source)
at com.apcc.m11.application.PicardApplication.verifyAndUpdateConfigFile(Unknown Source)
at com.apcc.m11.application.PicardApplication.createPermanentStorage(Unknown Source)
at com.apcc.m11.application.PicardApplication.main(Unknown Source)
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] Created thePermanentStorage
2017-03-02 19:41:26,139 [PcbeHSM-EventDispatcher] INFO - [AgentHSM.AgentHsm] State Change InitialState -> ActiveState
2017-03-02 19:41:27,155 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:28,171 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:29,188 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:30,204 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:31,220 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:32,235 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:33,252 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:34,268 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:35,283 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false

Attachments
esekh_apc
Crewman
Crewman
0 Likes
0
333

Re: Serial Communication with APC UPS RM 750 (SMT750RMI2U)

This was originally posted on APC forums on 3/3/2017


I do it recommendation for clear:

http://www.apc.com/us/en/faqs/index?page=content&id=FA159894&actp=search&viewlocale=en_US&searchid=1...

And after reinstall now all ok.

Thanks.

hopto_apc
Cadet
0 Likes
0
333

Re: Serial Communication with APC UPS RM 750 (SMT750RMI2U)

This was originally posted on APC forums on 5/21/2019


Hello, can u help me? My smt750i can`t connect with my PC over serial port, but ur program showing this.

Attachments
BillP
Administrator Administrator
Administrator
0 Likes
0
334

Re: Serial Communication with APC UPS RM 750 (SMT750RMI2U)

This reply was originally posted by Bill on APC forums on 5/22/2019


Hello,

What software are you trying to connect to the the UPS over serial comm? If anything other than PowerChute Business Edition it is not supported. If PowerChute Business Edition is failing to discover the UPS over serial comm what version of PowerChute are you installing?