Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-28 05:45 AM
This was originally posted on APC forums on 2/28/2017
Try connect to APC UPS RM 750 (SMT750RMI2U) via serial interface and cable that was with device 940-625A. Used real COM1 port where OK work early old my UPS SMART 1000.
I try to use software:
But device not detected. COM Port not answer.
By post :
I have information that SMT750 should work with serial port in any case.
When i test to use with USB connection PowerChute Business 9.2 detect ups OK .
I manual described that can work or serial or USB connection in one time. May be need switch by some procedure ?
Factory reset not help in my case.
SN: AS1621241318
Posted: 2021-06-28 05:45 AM
This reply was originally posted by Bill on APC forums on 5/22/2019
Hello,
What software are you trying to connect to the the UPS over serial comm? If anything other than PowerChute Business Edition it is not supported. If PowerChute Business Edition is failing to discover the UPS over serial comm what version of PowerChute are you installing?
Posted: 2021-06-28 05:45 AM
This was originally posted on APC forums on 3/3/2017
Thanks for SerialTerm.exe. By this apps I detected wrong MB cable connector. They was with other order of pins.
And now I know that new SMART-UPS use SPEED 9600.8.n.1.n, with old SMART-UPS used speed 2400.8.n.1.n
At image show order of pins.
But now other problem with start Agent.
After many reinstall of program agent 9.2, now not started service of PowerChute Business Edition Agent.
7024 | Error | Microsoft-Windows-Service Control Manager | System | 03.03.2017 4:20:05 |
The APC PBE Agent service terminated with the following service-specific error: The operation completed successfully.
101 | Error | APCPBEAgent | Application | 03.03.2017 4:20:04 |
Error: 0, Time out 90 seconds. Service start operation canceled.
But early at this host agent started correctly.
It link not resolve same problem.
Server Core HV-2016. USB connection. APC UPS RM 750.
Logs: pcbe.log
2017-03-02 19:41:26,108 [main] INFO - [application.PicardApplication] - Legacy logging adapter enabled.
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] Java Runtime: Java(TM) SE Runtime Environment (ve
rsion: 1.8.0_31)
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] Java Home: C:\PROGRA~2\APC\POWERC~1\JRE18~1.0_3
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] JVM: Java HotSpot(TM) Client VM (version: 25.31-b
07)
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] OS: Windows Server 2012 (x86)
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] Time Zone: Europe/Helsinki
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] PCBE dir: C:\PROGRA~2\APC\POWERC~1\agent
2017-03-02 19:41:26,124 [main] ERROR - [application.PicardApplication] Can not read M11.cfg file:
java.io.FileNotFoundException: m11.cfg (The system cannot find the file specified)
at java.io.FileInputStream.open(Native Method)
at java.io.FileInputStream.
at java.io.FileInputStream.
at com.apcc.m11.application.PicardApplication.verifyAndUpdateConfigFile(Unknown Source)
at com.apcc.m11.application.PicardApplication.createPermanentStorage(Unknown Source)
at com.apcc.m11.application.PicardApplication.main(Unknown Source)
2017-03-02 19:41:26,124 [main] INFO - [application.PicardApplication] Created thePermanentStorage
2017-03-02 19:41:26,139 [PcbeHSM-EventDispatcher] INFO - [AgentHSM.AgentHsm] State Change InitialState -> ActiveState
2017-03-02 19:41:27,155 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:28,171 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:29,188 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:30,204 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:31,220 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:32,235 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:33,252 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:34,268 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
2017-03-02 19:41:35,283 [main] INFO - [application.PicardApplication] isStartupComplete() - returns: false
Posted: 2021-06-28 05:45 AM
This was originally posted on APC forums on 3/3/2017
I do it recommendation for clear:
And after reinstall now all ok.
Thanks.
Posted: 2021-06-28 05:45 AM
This reply was originally posted by Bill on APC forums on 5/22/2019
Hello,
What software are you trying to connect to the the UPS over serial comm? If anything other than PowerChute Business Edition it is not supported. If PowerChute Business Edition is failing to discover the UPS over serial comm what version of PowerChute are you installing?
User | Count |
---|---|
4834 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.