Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79268members
343914posts

Send SMS from SNMP AP9631 issue

Solved
matthew.nq_apc
Ensign
Ensign
0 Likes
1
168

Send SMS from SNMP AP9631 issue

This was originally posted on APC forums on 10/25/2016


Hello

I have two SRT5KXLI ups,which i must make these two UPS send alerts (Warnings,Critical,information) via GSM modem.

What are the requirements to setting up this action,including hardware(GSM-Modem brand which is compatible with the NMC of UPS) and the physical connection between modem & SNMP card (AP9631),and software to done these actions?
Could you please help me to implementation of this that works fine?

Regards

Tags (3)

Accepted Solutions
matthew.nq_apc
Ensign
Ensign
0 Likes
0
168

Re: Send SMS from SNMP AP9631 issue

This was originally posted on APC forums on 10/26/2016


Anybody?!frown

See Answer In Context

1 Reply 1
matthew.nq_apc
Ensign
Ensign
0 Likes
0
169

Re: Send SMS from SNMP AP9631 issue

This was originally posted on APC forums on 10/26/2016


Anybody?!frown