Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79532members
344359posts

SYMETRA PX 80KVA

Solved
problemsolver_apc
Cadet
0 Likes
1
76

SYMETRA PX 80KVA

This was originally posted on APC forums on 2/11/2009


Hi,

We've had the APC in row cooling system now for about 8 months. One of the problems we've experienced right from the start was with the static switch. It has been replaced 3 times and I was wondering if anyone else had experineced the same problems.

Thanks


Accepted Solutions
dgordon_apc
Crewman
Crewman
0 Likes
0
76

Re: SYMETRA PX 80KVA

This was originally posted on APC forums on 2/23/2009


I am on my 3rd static switch and I finally made them replace the entire frame. In the first frame they found some type of liquid\oil substance dripping out of the communications bay and killed the first 2. The new frame had 1 in it and it appreas to be working fine, although they had issues starting it up. There was a problem with the communication card in the switch.

See Answer In Context

1 Reply 1
dgordon_apc
Crewman
Crewman
0 Likes
0
77

Re: SYMETRA PX 80KVA

This was originally posted on APC forums on 2/23/2009


I am on my 3rd static switch and I finally made them replace the entire frame. In the first frame they found some type of liquid\oil substance dripping out of the communications bay and killed the first 2. The new frame had 1 in it and it appreas to be working fine, although they had issues starting it up. There was a problem with the communication card in the switch.