Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-07-07 11:23 PM
This was originally posted on APC forums on 8/12/2015
Hi,
I have some problem with ordering of the new batteries for this device and the old one's completely unusable. Is it possible to turn off somehow that per second beeping? I have this message in my log: "UPS: The battery is not installed properly" and battery indicator blinking (on the front panel).
Regards,
Posted: 2021-07-07 11:24 PM
This reply was originally posted by Angela on APC forums on 8/13/2015
Hi Alex,
If that option doesn't disable the beep for your situation, then there won't be a way to. Like I said, we don't typically allow this type of thing since the batteries are a crticial part of the UPS functioning so we want to constantly remind (annoy) the user or else they have no battery back up. I suggested double checking it since I did see a different UPS, one with SUA model prefix, seemed to apply this setting and mute this disconnected battery beep going against what I just said
Unfortunately too, online models like SURT (and SRT) models need good batteries to turn on. You'll need to get it some good batteries to get it turned on again. I'd say put it in bypass as other models would work like that but this model has an electronic bypass so it would also require good batteries to engage the bypass function.
Posted: 2021-07-07 11:23 PM
This reply was originally posted by Angela on APC forums on 8/12/2015
I am not 100% sure if that specific alarm can be disabled but critical battery alarms like that typically cannot be since the battery is the lifeblood of the UPS. If there is any chance of disabling it, you'd see the option within the UPS Network Management Card menu with the other UPS options. Do you have access to that management card? This UPS would include one by default.
Posted: 2021-07-07 11:23 PM
This was originally posted on APC forums on 8/13/2015
Of couse I have an access, I'm using it an every day, but I just can't find there the option which could be used to disable it. A lot of network equipments give's more functionality with CLI. I thought that if it's possible, it should be a special command to disable it. But I am not sure about that, maybe it's completely impossible, that's why I'm asking.
Posted: 2021-07-07 11:24 PM
This was originally posted on APC forums on 8/13/2015
I have AP9631 model. I had set "Never" in that option already but it's still beeping. There was a power loss an hour ago, since that I can't turn on the UPS. I think that's because all batteries was unplugged. Is it possible to turn it on without batteries?
Thank you for your help!
Posted: 2021-07-07 11:24 PM
This reply was originally posted by Angela on APC forums on 8/13/2015
Hi Alex,
If that option doesn't disable the beep for your situation, then there won't be a way to. Like I said, we don't typically allow this type of thing since the batteries are a crticial part of the UPS functioning so we want to constantly remind (annoy) the user or else they have no battery back up. I suggested double checking it since I did see a different UPS, one with SUA model prefix, seemed to apply this setting and mute this disconnected battery beep going against what I just said
Unfortunately too, online models like SURT (and SRT) models need good batteries to turn on. You'll need to get it some good batteries to get it turned on again. I'd say put it in bypass as other models would work like that but this model has an electronic bypass so it would also require good batteries to engage the bypass function.
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.