Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80592members
346511posts

SURT10000XLT Run-time calibration

fishkillr_apc
Crewman
Crewman
0 Likes
0
88

SURT10000XLT Run-time calibration

This was originally posted on APC forums on 12/24/2015


SURT10000XLT,  SN:NS0623003696

Rack mount unit with 4 XR battery cabinets, with a total of 10 recently replaced RBC44 battery modules. The unit is not reporting the correct run-time. It's backing up some critical equipment that we are un-able to shut down so we would like to re-set the battery constant as outlined in the APCUPSD manual. We've been successful in doing this before, on smaller SU's, using the values in the manual. There isn't a value listed for an SURT10000XLT but there is one for an SURT10000XLI. Can I use the XLI value for the XLT? If not can you PM me the correct value? 

Thanks,

Jim