Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80614members
346550posts

SUA1000i cold start gives Overload warning with nothing attached

Solved
aneng_apc
Cadet
0 Likes
1
90

SUA1000i cold start gives Overload warning with nothing attached

This was originally posted on APC forums on 6/15/2010


Hi, My SUA1000i will not cold start properly - it tries to, then gives a continuous beep with a red overload light - but there is nothing at all attached to the UPS ! Running a self-test via Powerchute results in a pass.

Why is it doing this ? I need to to cold start for an oddball application (i.e. an extremely low power load (<10 watts) in a location that has no mains electricity). I can find no mention of the warning or the cold start procedure in the manual.

Any ideas ???


Accepted Solutions
bogdangepe_apc
Ensign
Ensign
0 Likes
0
90

Re: SUA1000i cold start gives Overload warning with nothing attached

This was originally posted on APC forums on 11/14/2016


I have the same problem. After a 10 - 20 times to start without power. 

See Answer In Context

1 Reply 1
bogdangepe_apc
Ensign
Ensign
0 Likes
0
91

Re: SUA1000i cold start gives Overload warning with nothing attached

This was originally posted on APC forums on 11/14/2016


I have the same problem. After a 10 - 20 times to start without power.