Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-27 11:49 PM
This was originally posted on APC forums on 2/24/2015
I have an SU3000RMT2U with a failed firmware upgrade. When attempting to upgrade the firmware via the management card, the LCD displayed the "Firmware upgrade in progress" message. I left it alone for over 24 hours at which point it was still displaying the message and the management card had no connection with the UPS.
I removed power (including battery disconnection) and it is now unresponsive. The LCD is backlit but displays nothing and does not respond to any buttons on the front. In addition, the serial port on the UPS is unresponsive.
Any thoughts or have I bricked this thing?
Posted: 2021-06-27 11:50 PM
This was originally posted on APC forums on 3/4/2015
Shoot. I was afraid of that. I suppose it's my fault for not being more careful. Time to go shopping for a new unit 🙂 I wonder what the going rate is for a bricked year-old 2200 on ebay...
Posted: 2021-06-27 11:49 PM
This reply was originally posted by Angela on APC forums on 2/24/2015
Hi Eric,
I'd review this post and see if my or David's suggestion works -> http://forums.apc.com/spaces/5/smart-ups-symmetra-lx-rm/forums/general/72/smart-ups-3000va-lcd-rm-2u...
Posted: 2021-06-27 11:50 PM
This was originally posted on APC forums on 2/24/2015
Thanks, Angela! Reviewing now and will report back.
Posted: 2021-06-27 11:50 PM
This was originally posted on APC forums on 2/26/2015
Angela,
I reviewed the post and tried the suggestions but it didn't work. Specifically, here is what I tried:
Thanks for any help you can provide.
Posted: 2021-06-27 11:50 PM
This reply was originally posted by Angela on APC forums on 2/26/2015
Hi Eric,
You connected @ 9600 baud rate, right? 9600, 8 data bits, parity non, stop bits 1, no flow control are the full port settings - I imagine so if you saw the wizard talking.
You don't happen to have any idea what the firmware was prior to the upgrade, do you? I learned today some of the earlier versions would fail an upgrade and only retry on the serial port so I'd say we'll likely have to focus on seeing if we can get the serial port upgrade working.
Last question - do you mind sharing where in the US you are?
Posted: 2021-06-27 11:50 PM
This was originally posted on APC forums on 2/28/2015
Hi Angela, I was on 09.1 prior to attempting the upgrade. I did try the settings you mentioned and also tried at 2400 baud. I'm in Denver, Colorado.
Posted: 2021-06-27 11:50 PM
This reply was originally posted by Angela on APC forums on 3/2/2015
Hi Eric,
I did some checking to make sure there was nothing else we could try - if you are not seeing any characters over the RJ-45 serial port connection at any of the port speeds (2400 or 9600), the UPS is likely bricked unfortunately and the bootloader isn't working to accept a file. If you were able to get that far, it would've been just like that post I linked to you and you could've sent the file over XMODEM and likely recovered.
Posted: 2021-06-27 11:50 PM
This was originally posted on APC forums on 3/4/2015
Shoot. I was afraid of that. I suppose it's my fault for not being more careful. Time to go shopping for a new unit 🙂 I wonder what the going rate is for a bricked year-old 2200 on ebay...
User | Count |
---|---|
4834 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.