Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80866members
346961posts

SMX3000 Internal fault message

MarkC_apc
Commander
Commander
0 Likes
0
164

SMX3000 Internal fault message

This was originally posted on APC forums on 8/17/2015


This is a follow-up of a post that I started several months ago (same title) requesting any experience with this excellent UPS having an "internal fault" message on the LCD screen, yet the unit worked fine in all respects being controlled through the NMC2 card.  Recently, after removing the NMC's "cage" to gain access to the microprocessor area and doing a little "probing", it was necessary to re-install the NMC to test a new router/D-Link repeater set up.  Upon startup of the UPS, the LCD screen now works as originally intended with full menu control. 

If anyone has had any type of similar experience with the SMX line, please post a reply.

P.S.  "probing" is not recommended by the manufacturers and is done at your own peril of damage to equipment and yourself!