Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80587members
346505posts

SMT1000RM2U no fan installed?

simpleace_apc
Ensign
Ensign
0 Likes
0
96

SMT1000RM2U no fan installed?

This was originally posted on APC forums on 3/25/2021


Hello everyone!

 

From my research it seems that the SMT1000 does not come with a fan built into the back rather the fans come installed on SMT1500 model and up.

 

Is this correct? Is that something that should be a concern? Is there a way or has anyone installed a fan back there to provide additional cooling for the unit?

 

Thanks!