Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80771members
346786posts

SMT 1000 access

Solved
dutch_apc
Cadet
0 Likes
3
230

SMT 1000 access

This was originally posted on APC forums on 6/4/2013


I have an SMT 1000 connected via USB to my WIN8/64 system.

In the past I have accessed the admin panel in a browser using http://127.0.0.1:3052/..

But the browser now responds with an "Unable to connect" error message.

I believe I was still on Win7 when last I accessed the admin panel via the browser.

Any suggestions?

Tags (3)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
230

Re: SMT 1000 access

This reply was originally posted by Angela on APC forums on 6/17/2013


I like those easy ones! laughing

See Answer In Context

3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
0
230

Re: SMT 1000 access

This reply was originally posted by Angela on APC forums on 6/4/2013


You can also try https://127.0.0.1:6547 or instead of the loopback, try the IP of the system (and you of course need to do that if you're on a different machine).

If that doesnt work, you'll want to go to the machine where the PowerChute Business Edition Agent is installed and view the running services via Administrative Tools->Services and verify the APC PBE Agent is present and actually running.

dutch_apc
Cadet
0 Likes
0
230

Re: SMT 1000 access

This was originally posted on APC forums on 6/16/2013


Thank you kindly for comment smile

Turns out I had had to reinstall the OS, and had forgotten to reinstall PowerChute.

It's running now, though I cannot update to V9.1 from V8.5 due to V9.1 not finding the unit on the USB.

But it functions and thats good smile

BillP
Administrator Administrator
Administrator
0 Likes
0
231

Re: SMT 1000 access

This reply was originally posted by Angela on APC forums on 6/17/2013


I like those easy ones! laughing