Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-29 04:50 AM
This was originally posted on APC forums on 10/24/2012
Is there a "like for like" replacement for the matrix 5000. We have three of them, and need three replacements but we can allow for runtime value to drop by 50%
Would the new UPS use the same "power out"connector as the matrix 5000 "power out"?
In these times please think cheap!
:-)
Posted: 2021-06-29 04:50 AM
This reply was originally posted by Angela on APC forums on 10/29/2012
it should give you your % W (wattage) and % VA (volt-amps) if supported. i think those headings would be present in the data log and maybe on the status screen.
do you see either of those values? My concern is if the 50% is wattage or VA because the matrix is 5000VA but can only supply 3750 watts as seen @ http://www.apc.com/resource/include/techspec_index.cfm?base_sku=MX5000
Posted: 2021-06-29 04:50 AM
This was originally posted on APC forums on 10/26/2012
Allow me demonstrate my ignorance by saying
"uk 240v" 🙂
Nothing particular special about the setup, so I am not sure if "step down" is needed.
I think we have come to the decision to replace it with
APC Smart-UPS RT 8000VA 230V (thanks for your advice)
One thing, if one of the old matrix 5000 were running at 50% power capacity does that mean that the load is 2500VA? How can I tell what the load is, I have a network card and can web into it, but it was not clear.
Posted: 2021-06-29 04:50 AM
This reply was originally posted by Angela on APC forums on 10/25/2012
the most direct replacement we'd have today would be the [Smart UPS RT line|http://www.apc.com/products/family/index.cfm?id=163]. problem is with those there is no isolation transformer like the matrix has so for 120v, you can add on an isolation transformer or a stepdown transformer for 120v.
which output voltages do you require?
Posted: 2021-06-29 04:50 AM
This reply was originally posted by Angela on APC forums on 10/29/2012
it should give you your % W (wattage) and % VA (volt-amps) if supported. i think those headings would be present in the data log and maybe on the status screen.
do you see either of those values? My concern is if the 50% is wattage or VA because the matrix is 5000VA but can only supply 3750 watts as seen @ http://www.apc.com/resource/include/techspec_index.cfm?base_sku=MX5000
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.