Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80827members
346902posts

Re: datacenter expert 7.9.0 upgrade

Jerome_C
Ensign
Ensign
0 Likes
0
114

Re: datacenter expert 7.9.0 upgrade

Well,

I had a reply from the support which says that there are some trouble with the build 192 of the 7.9.0 version.

We will try the build 196 in a couple of weeks.

 

Jerome

 

Tags (1)