Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80622members
346574posts

Powerchute Personal Edition 3_0_2 and Blackout time

Solved
Tibbie_apc
Cadet
0 Likes
1
113

Powerchute Personal Edition 3_0_2 and Blackout time

This was originally posted on APC forums on 2/6/2015


Hi

Using this software in the UK and the time it reports after an event is incorrect, does the Personal Edition not support changing the time zone, quite a basic requirement really ??

Thanks

Tags (3)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
113

Re: Powerchute Personal Edition 3_0_2 and Blackout time

This reply was originally posted by Bill on APC forums on 2/9/2015


Nick,

PowerChute Personal Edition pull the date and time from the system clock. Example: I am in the U.S. in the Eastern time zone. I installed PCPE on Windows 7 home edition with the system clock set the (UTC -5:00) Eastern Time (US & Canada) I turned the power off the the UPS and restored after 60 seconds. PCPE reported the outage at 10:07. I then changed the system clock to (UTC) Dublin, Edinburgh, Lisbon, London and restarted the system. After restarting I turn the power of the the UPS and restored after 60 seconds. PCPE reported the outage at 15:13

Hope this info helps.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
114

Re: Powerchute Personal Edition 3_0_2 and Blackout time

This reply was originally posted by Bill on APC forums on 2/9/2015


Nick,

PowerChute Personal Edition pull the date and time from the system clock. Example: I am in the U.S. in the Eastern time zone. I installed PCPE on Windows 7 home edition with the system clock set the (UTC -5:00) Eastern Time (US & Canada) I turned the power off the the UPS and restored after 60 seconds. PCPE reported the outage at 10:07. I then changed the system clock to (UTC) Dublin, Edinburgh, Lisbon, London and restarted the system. After restarting I turn the power of the the UPS and restored after 60 seconds. PCPE reported the outage at 15:13

Hope this info helps.