Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80877members
346974posts

PowerChute V9.1.0 does not recognize USB attached Smart-UPS

Solved
BillP
Administrator Administrator
Administrator
0 Likes
3
162

PowerChute V9.1.0 does not recognize USB attached Smart-UPS

This question was originally posted by Jim on APC forums on 7/31/2013


Ok ... I have an older PC that performs environmental supervision for a remote site.

It runs XP Professional SP3 with all security patches.

I just upgraded from an older version of PowerChute to the latest PowerChute V9.1.0, and aquired a newer SmartUPS 1500

PowerChute does not recognize the UPS

USB connection seems OK as when I plug the UPS in to the PC with the PC running,

the UPS is recognized as an HID-type device - named:  "American Power Conversion USB UPS"

This device gets removed from Device manager when I unplug the USB cable

I checked Microsoft update and it asserts no newer device driver is available for the device

When I launch the web interface for the PowerChute (Business Edition) Agent s/w via:  http://127.0.0.1:3052

the interface tells me the device is not connected.

When I go to Server Shutdown --> System Settings --> Device Communications Port

It only offers COM1 or COM3 - not a USB type connection....

What have I done wrong?


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
162

Re: PowerChute V9.1.0 does not recognize USB attached Smart-UPS

This reply was originally posted by Bill on APC forums on 7/31/2013


You need to uninstall the PowerChute Agent and reinstall it. I assume that the newer Smart-UPS you are using is either a SMT or SMX model and those models have a different communication protocol than older Smart-UPS did.  By uninstalling and reinstalling PowerChute will recognize the newer Smart-UPS and establish communications.

See Answer In Context

3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
0
163

Re: PowerChute V9.1.0 does not recognize USB attached Smart-UPS

This reply was originally posted by Bill on APC forums on 7/31/2013


You need to uninstall the PowerChute Agent and reinstall it. I assume that the newer Smart-UPS you are using is either a SMT or SMX model and those models have a different communication protocol than older Smart-UPS did.  By uninstalling and reinstalling PowerChute will recognize the newer Smart-UPS and establish communications.

BillP
Administrator Administrator
Administrator
0 Likes
0
162

Re: PowerChute V9.1.0 does not recognize USB attached Smart-UPS

This reply was originally posted by Jim on APC forums on 7/31/2013


Thanks Bill ... The unit I am using is a few years old it is a Model DLA1500 ....

I don't know which communications protocol it uses, so I'll uninstall/reinstall and report back ....

Thanks!

BillP
Administrator Administrator
Administrator
0 Likes
0
162

Re: PowerChute V9.1.0 does not recognize USB attached Smart-UPS

This reply was originally posted by Jim on APC forums on 7/31/2013


Thanks Bill that fixed it!

I might suggest to the programming team they they create a "search for UPS" option within powerchute,

or prompt during upgrade-installs to ask if user would like to uninstall old version first

(either as part of install, or warn of circumstances where-in user might want to manually uninstall prior to installation of new version)