Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80833members
346908posts

PDU firmware upgrade

Dominique38
Cadet
Cadet
0 Likes
2
158

PDU firmware upgrade

Hi,

 

Is there any "official" document saying that PDU firmware upgrade will not/never swtich output during/after upgrade process ?

thanks.

Tags (1)
2 Replies 2
TonKei
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
1
154

Re: PDU firmware upgrade

Hi

 

This subject has been discussed in a previous, that you can find here -> https://community.exchange.se.com/t5/EcoStruxure-IT-forum/Do-firmware-updates-require-reboots/td-p/2...

 

The short version is:

"For any devices, including Rack PDU, as long as they are operating normally and you have no active alarms we should check prior, a firmware upgrade of the management interface done through any method, including DCE, will not power on/off any attached loads."

 

But, as discussed in the post, there are fault states, that when active in the PDU, can cause the PDU to stop delivering power.

 

Best regards

Tonny

Tags (1)
Dominique38
Cadet
Cadet
0 Likes
0
123

Re: PDU firmware upgrade

Thanks your answer.

So, why not writing an official document saying same thing ??

Tags (1)