Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80811members
346876posts

PCNS shuts down all hosts instead of two

Solved
DotB_apc
Cadet
0 Likes
2
93

PCNS shuts down all hosts instead of two

This was originally posted on APC forums on 7/25/2017


PCNS shuts down all hosts instead of two

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
94

Re: PCNS shuts down all hosts instead of two

This reply was originally posted by Bill on APC forums on 7/25/2017


Hi,

You will find a description of how to configure PCNS for multiple sites in Application Note 180. The recommendation is to have PCNS running on a stand alone Windows system at each site. vCenter Server should also be running on a stand alone Windows system at one of the four sites. PCNS and vCenter can be running as VMs but that is not the recommended configuration. 

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
95

Re: PCNS shuts down all hosts instead of two

This reply was originally posted by Bill on APC forums on 7/25/2017


Hi,

You will find a description of how to configure PCNS for multiple sites in Application Note 180. The recommendation is to have PCNS running on a stand alone Windows system at each site. vCenter Server should also be running on a stand alone Windows system at one of the four sites. PCNS and vCenter can be running as VMs but that is not the recommended configuration. 

DotB_apc
Cadet
0 Likes
0
94

Re: PCNS shuts down all hosts instead of two

This was originally posted on APC forums on 8/15/2017


Hi,

thank you for your quick response.

We now deployed a seperate PCNS Appliance for every site without physical hosts and a PCNS Client with VMware Support for every site that has a physical host.

Unfortunately I wont have the chance to test the deployment soon.

But I will report the outcome when tests have been made.

Kind Regards