Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79472members
344251posts

PCNS 4.2 not available after deploy

BillP
Administrator Administrator
Administrator
0 Likes
0
33

PCNS 4.2 not available after deploy

This question was originally posted by Marco on APC forums on 11/7/2017


Hi,

i have a vCenter 6.5 and two ESXi Host 6.5. I want to shutdown these with PCNS Virtual Appliance.

- I deploy the Appliance

- I configure the network

- I boot the Appliance

- I set the unix password

But i am not able to connect over "https://ip:6547" or "https://ip:5480" also i can't ping the appliance......

I have installed the appliance several times but i get every the same result!?

My network is ok and all other machines reachable.

Thanks!

Edit: Solved! The Switch was the problem