Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79193members
343731posts

PCBE Reports Agent As "OLD"

Solved
foremansllp_apc
Cadet
0 Likes
1
111

PCBE Reports Agent As "OLD"

This was originally posted on APC forums on 1/10/2012


I have PCBE 9.0.1 installed with v9.0.1.606 agents installed on Server 2003.

When I run a Risk Assessment from the console I get a warning that I have "Old Agents" but I can't find an updated version of the agent anywhere.

Am I missing a download somewhere or is this a known problem ?


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
111

Re: PCBE Reports Agent As "OLD"

This reply was originally posted by Angela on APC forums on 1/10/2012


hello,

yes, this is a known issue. it will be fixed in 9.1. if you want to disable auto updates, you can get rid of the nuisance or just know that it is a known issue.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
112

Re: PCBE Reports Agent As "OLD"

This reply was originally posted by Angela on APC forums on 1/10/2012


hello,

yes, this is a known issue. it will be fixed in 9.1. if you want to disable auto updates, you can get rid of the nuisance or just know that it is a known issue.