Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-30 10:22 PM
This was originally posted on APC forums on 3/30/2016
PBE Console cannot establish network communication with UPS. However, the Web Agent communicates successfully.
I have a Smart-UPS 1500 protecting a single Desktop PC running Windows 10. Connection to UPS is via USB. Windows Device Manager correctly finds and identifies the UPS.
I have tried editing the java.security file mentioned in some posts, but this has not resolved the problem.
Any suggestions would be appreciated.
Posted: 2021-06-30 10:23 PM
This was originally posted on APC forums on 3/30/2016
Thanks so much. That fixed it (removing and then re-adding the Agent in Console). Cheers --Mike
Posted: 2021-06-30 10:23 PM
This reply was originally posted by Bill on APC forums on 3/30/2016
Hi,
Verify that the PowerChute Server is using the same user name and password and the PowerChute Agent. When installing the PowerChute Agent you are required to enter a user name and password. The when installing the PowerChute Server you are again asked to enter a user name and password. If those do not match the PowerChute Server will not discover the Agent.
You can change the user name and password for the PowerChute Server in the Console. Go to Tools - Change User Name/password
If the Agent is displayed in the console with UPS Communication Lost and you can access the Agent via the web interface and it show communicating with the UPS you should
1 - In the Console go to Tools - Configuration Device List and remove the Agent and click apply. Then re-add the Agent and click apply.
2 - If step 1 does not resolve the issue stop and the restart the Agent service. Open a command prompt as an administrator and enter net stop apcpbeagent. After the service stops restart it. The command is net start apcpbeagent.
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.