Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79503members
344312posts

Only one Smart UPS 3000 System recognized by PC - Connected through USB

Solved
Andrew.Posey_apc
Cadet
0 Likes
1
86

Only one Smart UPS 3000 System recognized by PC - Connected through USB

This was originally posted on APC forums on 5/24/2016


Hello,

I'm trying to set up monitoring for four Smart UPS 3000 systems on a single Windows 7 PC. When I connect all systems to the PC and run a search through USB, it only finds one system.

 

Is there any way to get all four connected through USB? Is it a simple setting I'm missing?

Thank you

Tags (3)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
86

Re: Only one Smart UPS 3000 System recognized by PC - Connected through USB

This reply was originally posted by Bill on APC forums on 5/25/2016


Hi,

You can only monitor 1 UPS at a time via USB. If you want to monitor 4 UPS from the same PC you should purchase network management cards for the Smart-UPS and then you can monitor the UPS via web interface, SSH, Telnet, or SNMP. 

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
87

Re: Only one Smart UPS 3000 System recognized by PC - Connected through USB

This reply was originally posted by Bill on APC forums on 5/25/2016


Hi,

You can only monitor 1 UPS at a time via USB. If you want to monitor 4 UPS from the same PC you should purchase network management cards for the Smart-UPS and then you can monitor the UPS via web interface, SSH, Telnet, or SNMP.