Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80612members
346542posts

Non-connected ap9617 cmos reset

Solved
bbailey_apc
Cadet
0 Likes
6
190

Non-connected ap9617 cmos reset

This was originally posted on APC forums on 6/3/2013


Is there anyway to reset the ap9617 to factory configuration without the ap9617 being in a UPS?  Removing the button battery does not clear the settings.

Thanks

Tags (1)

Accepted Solutions
Battman_apc
Commander
Commander
0 Likes
0
190

Re: Non-connected ap9617 cmos reset

This was originally posted on APC forums on 6/3/2013


I've done work on these cards with them installed in an AP9600 smartslot expansion chassis powered by a 24 vdc adapter...that's the only way to both power them and access them serially that I know of.

See Answer In Context

6 Replies 6
bbailey_apc
Cadet
0 Likes
0
190

Non-connected ap9617 cmos reset

This was originally posted on APC forums on 6/3/2013


Is there anyway to reset the ap9617 to factory configuration without the ap9617 being in a UPS?  Removing the button battery does not clear the settings.

Thanks

Battman_apc
Commander
Commander
0 Likes
0
191

Re: Non-connected ap9617 cmos reset

This was originally posted on APC forums on 6/3/2013


I've done work on these cards with them installed in an AP9600 smartslot expansion chassis powered by a 24 vdc adapter...that's the only way to both power them and access them serially that I know of.

Battman_apc
Commander
Commander
0 Likes
0
191

Re: Non-connected ap9617 cmos reset

This was originally posted on APC forums on 6/3/2013


...and what happens when the button battery dies ?   (something I've been meaning to find out for some time now !). ...Thanks!

bbailey_apc
Cadet
0 Likes
0
191

Re: Non-connected ap9617 cmos reset

This was originally posted on APC forums on 6/3/2013


Just a quick follow-up question.  What is the purpose of the button battery on the ap9617?

BillP
Administrator Administrator
Administrator
0 Likes
0
191

Re: Non-connected ap9617 cmos reset

This reply was originally posted by Angela on APC forums on 6/3/2013


It just keeps the date and time. I guess then if it fails just the date and time would reset when the card removed from power. I thought that for this type of application these would last upwards of 10 years potentially so then it might be time for an upgrade if it does die smile - it is not designed to be replaceable. On the newer cards it does not just 'pop out' but I think it might on the AP9617/18/19.

stevejenkins_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
191

Re: Non-connected ap9617 cmos reset

This was originally posted on APC forums on 6/30/2013


Arrgghhh.... Found this thread after searching and hoping that removing the battery from an AP9617 might reset the config. Time to go find my serial cable. smile