Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79186members
343707posts

Model number required for below specificartion

Solved
BillP
Administrator Administrator
Administrator
0 Likes
1
132

Model number required for below specificartion

This question was originally posted by Anup on APC forums on 12/8/2015


Hi All,

please help me with the model number which support below features in APC rack,

Rack will have to be standard of 42 Or by 19 inches, of the same brand that the manufacturer of the server. In addition it will have to count on:

 

  • front door of material transparency for visual supervision of equipment, equipped with security key,
  • 1 (one) sweeps for the feedings 220VAC of the equipment, this bar must have leftover takings like minimum 20% of the total of

takings,

  • 2 (two) bars of earth with size nonsmaller to 48.26 cm in length, 5 cm in width and 0,5cm of thickness, this would install in the party inferior of rack, one ahead and the other behind rack.
  • 4 (four) strips of power supply for 220 volts, with independent heat screen, in addition must have leftover takings as minimum 20% of the total of takings. The type of taking will have to correspond to the card type of connection of the equipment that will be installed in rack.
  • rack will have to be equipped with factory air extractor, like minimum two extractors by rack of sizes nonsmaller to 10cm x

10cm.

· Also will be due to anticipate two to cosmell by rack of spare part of the size and equal characteristics to the installed ones in rack


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
132

Re: Model number required for below specificartion

This reply was originally posted by Bill on APC forums on 12/8/2015


Anup,

If you are in need of a rack that is the same brand as the server manufacture you should contact the server manufacture for assistance. 

We do manufacture racks and the information for those racks can be found at this link

http://www.apc.com/shop/us/en/categories/racks-and-accessories/_/N-1biii1l 

Here is a link to the SX rack specification PDF

http://www.apcmedia.com/salestools/ETOL-6VLMH2/ETOL-6VLMH2_R5_EN.pdf?sdirect=true

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
133

Re: Model number required for below specificartion

This reply was originally posted by Bill on APC forums on 12/8/2015


Anup,

If you are in need of a rack that is the same brand as the server manufacture you should contact the server manufacture for assistance. 

We do manufacture racks and the information for those racks can be found at this link

http://www.apc.com/shop/us/en/categories/racks-and-accessories/_/N-1biii1l 

Here is a link to the SX rack specification PDF

http://www.apcmedia.com/salestools/ETOL-6VLMH2/ETOL-6VLMH2_R5_EN.pdf?sdirect=true