Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79125members
343515posts

Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

Solved
neocodesoftware_apc
Crewman
Crewman
0 Likes
7
3514

Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

This was originally posted on APC forums on 2/14/2013


Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

Mac specs: Mac Pro, 2.8ghz quad core intel, 12gb ram, OS X Server 10.7.5
UPS specs: APC Smart-UPS SC1000 2U Rackmount Tower
Purchase date: Jan 2012
USB Cable: APC USB to Serial Smart Signaling Cable Model AP9833

#1 Using the System Information App USB section I can see that the Mac recognizes the cable as a USB-Serial Controller "Prolific Technology"

#2 The energy saver control panel does not display any UPS info and the System Information App Power section does not display any UPS info.

#3 We have tried unplugging the cable.

#4 We have tried installing apcupsd (which we use on our all linux boxes) - but it can not detect the UPS

Suggestions?


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
3514

Re: Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

This reply was originally posted by Angela on APC forums on 2/19/2013


did you ever get a driver for that prolific device? i've never used it on a Mac but I know on Windows it requires a driver to be installed. is the Mac indicating it is installed properly or did it just detect it and we might need a driver? i asked someone about this and they seemed to indicate that it is the same case on the Mac - driver needed.

See Answer In Context

7 Replies 7
neocodesoftware_apc
Crewman
Crewman
0 Likes
0
3515

Re: Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

This was originally posted on APC forums on 2/28/2013


um - no. no success.

tried installing the prolific drivers - and rebooted - no luck.

shutdown the mac and power cycled the UPS - no luck.

I tried this on two different Macs running different OS X versions.

gave up - ordered UPS from another vendor.

I still like APC just not Mac compatible for me.

BillP
Administrator Administrator
Administrator
0 Likes
0
3515

Re: Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

This reply was originally posted by Angela on APC forums on 2/28/2013


Sorry frown

neocodesoftware_apc
Crewman
Crewman
0 Likes
0
3515

Re: Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

This was originally posted on APC forums on 2/15/2013


wow!! fast reply!! thanks.

will try it and post back.

much appreciated.

i made these pictures of what i am going to try.

Message was edited by: neocodesoftware

Attachments
BillP
Administrator Administrator
Administrator
0 Likes
0
3515

Re: Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

This reply was originally posted by Angela on APC forums on 2/15/2013


the AP9833 is only a USB to serial adapter. you will still need the UPS communication cable that came with your UPS.

i believe your SC1000 came with a serial cable, part number 940-0024 or 940-1524, correct? it has a serial connector on both ends.

i think what you should have here is SC1000->940-0024/940-1524 serial cable->DB-9 end of AP9833->AP9833 USB end to your server.

can you try it this way and share results?

neocodesoftware_apc
Crewman
Crewman
0 Likes
0
3515

Re: Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

This was originally posted on APC forums on 2/19/2013


we tried this without success

we daisy chained the two cables together but no luck

i rebooted the mac no luck

the mac detects the usb cable but that's all

anything else to try or is it time to move to a new ups?

BillP
Administrator Administrator
Administrator
0 Likes
0
3515

Re: Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

This reply was originally posted by Angela on APC forums on 2/18/2013


looks good!

BillP
Administrator Administrator
Administrator
0 Likes
0
3515

Re: Mac OS X Server 10.7 computer doesn't display UPS options in Energy Saver

This reply was originally posted by Angela on APC forums on 2/19/2013


did you ever get a driver for that prolific device? i've never used it on a Mac but I know on Windows it requires a driver to be installed. is the Mac indicating it is installed properly or did it just detect it and we might need a driver? i asked someone about this and they seemed to indicate that it is the same case on the Mac - driver needed.