Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79539members
344373posts

[Java error]PowerChute Configuration

Solved
BillP
Administrator Administrator
Administrator
0 Likes
2
112

[Java error]PowerChute Configuration

This question was originally posted by amobile on APC forums on 1/30/2008


hello all,

i've got some problems with the installation of the PowerChute Configuration Software on my Linux server (Fedora 😎
I've install PowerChute for Linux distrib from the CDROM.
Installation done without any error.
When i try to launch the Configuration utility, i use the command written in the documentation:

java -cp m11.jar:confutil.jar:../comp/Notifier.jar:..comp/
CommandFileRunner.jar PCNSUtilApp

or

Java home dir\bin\java -cp m11.jar:confutil.jar:../comp/Notifier.jar:../comp/
CommandFileRunner.jar PCNSUtilApp

both doesn't work 😞
Error message return:

Configuration Utility Error: java.lang.NullPointerException

It's not a problem with my PATH.
My Java version is

java -version
java version "1.6.0_04"
Java(TM) SE Runtime Environment (build 1.6.0_04-b12)
Java HotSpot(TM) Server VM (build 10.0-b19, mixed mode)

Someone can help me?

Thanks a lot 🙂


Accepted Solutions
EZ_Button_apc
Commander
Commander
0 Likes
0
112

Re: [Java error]PowerChute Configuration

This was originally posted on APC forums on 1/30/2008


What software and version are you trying to install on this system?

See Answer In Context

2 Replies 2
grayloon_apc
Cadet
0 Likes
0
114

Re: [Java error]PowerChute Configuration

This was originally posted on APC forums on 6/19/2008


I get this error too with PowerChute 2.2.3 under MacOS X 10.4.11 PPC.

EZ_Button_apc
Commander
Commander
0 Likes
0
113

Re: [Java error]PowerChute Configuration

This was originally posted on APC forums on 1/30/2008


What software and version are you trying to install on this system?